Scheduled Reports Overview - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

Each scheduled report contains one or more properties (for example, Item Name and Status) of each item in an Object List. A report engine on the server runs the Scheduled Report at the specified times and saves it to a file in a standard location on the server. The report engine can also send the report output to a printer if specified.

There are two scheduled report screens: the Create New Scheduled Report Screen and the Scheduled Reports Viewer screen.