Configuring the Y-axis - Metasys - LIT-12011942 - "" - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

About this task

To configure the Y-axis in the Chart view:

Procedure

  1. Place your cursor on the chart and right-click.
  2. Select the Y-axis Scale menu item. The Range Configuration dialog box appears.
  3. If you are using stacked Y-axis, choose the trend item to which the Y-axis range should be applied from the item drop-down list.
  4. Specify whether to Use Automatic Range Calculation. The Range is determined automatically based on the trend items.
    Note: When you select Use Automatic Range Calculation, you do not fill in the Range fields.
  5. Specify the minimum and maximum values for the Y-axis.
    Note: When you use stacked Y-axis, click Apply to apply the changes to a specific trend item. You can continue setting the ranges for other trend items in the Range Configuration dialog box.
  6. Click OK.