Configuring the X-axis - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

About this task

To configure the X-axis in the Chart view:

Procedure

  1. Place your cursor on the chart and right-click.
  2. Select the X-axis Scale. The Range Configuration dialog box appears.
  3. Specify whether to Use Automatic Range Calculation. The automatic range is determined automatically based on the set-up in the Definition View.
    Notes:
    • You are limited to dates and times between the start and end dates configured in the Trend Study definition.
    • When you select Use Automatic Range Calculation, you do not fill in the Range fields.
  4. Specify the Start Time, Start Date, End Time, and End Date.
  5. Click OK.

Results

Note: You can also configure the X-axis range by changing the start and end dates and times in the Definition View. See the table in the Trend Study Definition View.