Configuring the ODS as the Destination for Trend Data - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

About this task

Notes:
  • You can define only one repository as the default destination.
  • If you need to provide long-term storage for trend samples from an Engine, follow these steps to configure the Trend Repository of an ODS as the Default Destination.

To configure the ODS Trend Repository as the Default Destination for trend samples from an Engine:

Procedure

  1. Select the Engine device in the navigation tree.
  2. View the Engine. See Displaying Information About an Item for more information on how to display an item.
  3. Select the Focus tab and click the Advanced radio button to display additional item information.
  4. Select Edit.
  5. Edit the ODS Repository and the ODS Delivery Time. (The Engine Device Object attributes table contains Default Value and Values/Options/Range information for the attributes.)
  6. Click Save.
    Note: If you want to define the ODS attributes for the entire site instead of at the individual Engine level, select the Site in the navigation tree and edit the ODS Repository and the ODS Delivery Time. (The Site Object attributes table contains Default Value and Values/Options/Range information for the attributes.)