Adding New Trend Items to the Trend Study - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

Procedure

  1. View the Trend Study.
  2. If necessary, click the Definition View button.
  3. Click the Edit button in the upper left of the Trend Study tab.
  4. Click the Add icon in the Trend Items table. The Select Item dialog box appears.
  5. Select the trend(s) that you wish to add from the Select Item dialog box.
    Notes:
    • Multiple selection adds multiple items.
    • All non-trend items appear dimmed. If everything appears dimmed in the Select Item dialog box, check to see if you have at least one object with a Trend Extension and/or that Engine devices from other sites are storing samples in the ODS (if applicable).
  6. Click the OK button in the Select Item dialog box.
  7. Click the Save button in the Definition View to save the changes.