Chart Right-Click Menu - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

You can access a right-click menu from the Chart view. Place your cursor in the chart and right-click in the panel to display the menu.

Table 1. Chart View Right-Click Menu

Menu Item

Description

Background Color

Opens the Select a Color dialog box and allows you to configure the background color.

Y-axis Scale

Displays the Y-axis Range Configuration dialog box.

X-axis Scale

Displays the X-axis Range Configuration dialog box.

Gridlines

Allows you to select what type of gridlines to appear on the chart. You can choose: None, X and Y, X Only, and Y Only.

Chart Type

Allows you to select what type of chart to display. You can choose: Points Line, Area, Bar, Points, and Line.

Stacked Y-axis

Displays the chart on a stacked Y-axis.