Default Destination - Metasys - LIT-12011942 - Software Application - ODS Server - 10.1

Metasys Open Data Server Help

Brand
Metasys
Product name
ODS Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14
Language
English

The ADS Repository defines where trend samples are sent when the local trend buffers reach their defined Transfer Setpoint (see the Trend Extensions section), the Engine defined ODS Delivery Time (see the Engine Device Object) is reached, or the user initiates a transfer. You can initiate a transfer by using the Trend Extension’s Route command.

Notes:
  • You do not need an ODS on the site to forward trends to an ODS. You can forward trend samples to an ODS on a different Metasys site. The off-site ODS that receives forwarded trend samples must be the Site Director of its site.
  • You can define only one repository as the default destination for each Engine.

For more information on ODS default trend destinations, see Configuring the ODS as the Destination for Trend Data.