Operating System - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

Engines use a Microsoft Windows Embedded or Linux operating system (specific operating system depends on the model), which is shipped preinstalled on the Engine or can be updated after the engine is installed. In general, the operating system cannot be modified by adding or deleting programs or drivers, although provisions are made to install factory-authorized patches and upgrades.