Flash Memory - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

A type of nonvolatile memory within the Engine device. The Engine stores the operating system, software, and archive within this memory. This memory is not used during normal operation of the Engine device, except when a new graphic is added and the new image is uploaded and stored. The flash memory is mostly used during shutdown and system restart.