Database - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

The database is the collection of objects and their parameters as defined by the user. Each database is unique to the job. A database can be created or edited (with appropriate user authority) either online using the Site Management Portal UI, or offline using SCT. SCT can also be used to download a database or upload and create a backup copy of the database.