Supervisory Device - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

Menu Selection: Insert > Supervisory Device

Inserts a supervisory device into the archive database with SCT, including the following network engines: NAE35, NIE39, NAE45, NAE451L, NIE49, NAE55, NIE59, NAE85, NIE89, NCE25, NIE29, NIE55, NIE85, SNE10/SNE11/SNE22, and SNC16/SNC25. You can insert a device at a previous Metasys system release with SCT, beginning with Release 5.2 and later. The SNE and SNC devices are only available to SMP at Release 10.1 or later, and SCT Release 13.2 and later.

Note: The NAE451L and SNE110L0 network engines are available only to select regions of Australia, China, Hong Kong, India, Indonesia, Japan, Korea, Malaysia, New Zealand, Philippines, Singapore, Taiwan, Thailand, Vietnam, and select branches.

On the Configure screen of this wizard, click any tabs that may appear for further device configuration.