This object contains attributes common to many Metasys system objects. These common attributes are described in the Common Object Attributes section. For information on the Tailored Summary feature, see the Tailored Summaries section in the Metasys SCT Help (LIT-12011964) .
Click the attribute name in the table for a description of the attribute.
|
Attribute Name |
Notes |
Initial Value |
Values/Options/Range |
Description |
|---|---|---|---|---|
|
Key Data |
C,N,W |
Limit of 4 key items |
Holds the item name or Fully Qualified Reference of a key item to display in a tailored summary. You can configure up to four key items. |
|
Attribute Name |
Notes |
Initial Value |
Values/Options/Range |
Description |
|---|---|---|---|---|
|
Column Definition |
C,W |
Column Heading, Child Item, Attribute |
Defines the columns displayed in a tailored summary. You can define up to seven columns (list of structures). Each structure contains the following information: Column Heading - Defines the name of the column header. Child Item - Indicates item for which the column data is retrieved based on its name attribute, which must match a user-specified pattern (such as ZN-* or ZN-T, Zone-T). To display an attribute of the row item, leave this field blank. Otherwise, specify the name of the child item to display. Attribute - Defines the attribute information for the column. The attributes are grouped into categories for easy selection. Select a category in the Attribute Filter section of the Select Column Attribute dialog, and then select the desired attribute from the list. |
|
|
Row Heading Column Text |
C,N,W |
Label Maximum: 50 characters |
Defines the text to display as the label for the row headings column (that is, the first column) in a tailored summary. |