Site Commands - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

The following table lists the commands supported by the Site Object.

Table 1. Site Object Commands

Command Name

Parameters

Description

Set Date

Day of Week/Month/Year

Sets the current date for the Site object.

Set Time

Hour:Minute:AM/PM

Sets the current time for the Site object.

Update Broadcast Management

None

Requests the system to select broadcast management devices over the Metasys network based on the Third Party BBMDs List attribute for determining BBMD devices.