Site - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

Menu Selection: Insert > Site

Inserts a site into the archive database in the SCT.

Tip: The Create Device? dialog box appears after inserting a site that asks if you want to create a device in the site. To invoke the Insert Device wizard, select Supervisory Device, then click OK. To invoke the Insert Metasys Server wizard, select Metasys Server, then click OK. If you do not want to add a device at this time, select None, then click OK.