This object contains attributes common to many Metasys system objects. These common attributes are described in the Common Object Attributes section. This section includes attributes of the Focus/Configuration tab, the Diagnostics tab (if applicable), and any other tab specific only to this object. See the Object and Feature Tabs section for information on the attributes that appear on the other tabs of this object (for example, the Hardware and Options tab appear on point objects).
Click the attribute name in the table for a description of the attribute.
|
Attribute Name |
Notes |
Initial Value |
Values/Options/Range |
|---|---|---|---|
|
Description of Halt |
|||
|
Enabled |
C,W |
||
|
Instance Of |
|||
|
Program Change |
W |
Ready |
0 = Ready 1 = Load 2 = Run 3 = Halt 4 = Restart 5 = Unload |
|
Program Location |
|||
|
Program State |
0 = Idle 1 = Loading 2 = Running 3 = Waiting 4 = Halted 5 = Unloading |
||
|
Reason for Halt |
0 = Normal 1 = Load Failed 2 = Internal 3 = Program 4 = Other |
||
|
Reliability |
Uses Reliability set. |