Program Object - Metasys - LIT-12011942 - Software Application - ODS Server - 10.1

Metasys Open Data Server Help

Brand
Metasys
Product name
ODS Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14
Language
English

The Program object (previously the Control System object) stores information needed for the user-defined control strategies created (graphically) with the Logic Connector Tool (LCT). The Control System object application now includes BACnet command object functionality and appears as the Program object in the Metasys software. The Program object attributes allow manipulation of the LCT application.

For general information on Metasys system objects, see Common Object Attributes.