Saving a Control System - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

To save a control system, click Save on the Toolbar. The LCT scans for logic errors.

Notes:

  • The logic check done with the Save command is not the same as the Logic Checker run from the toolbar.
  • If inputs are missing, an error message appears asking if you want to continue with the save. Click No to return to the logic. Click Yes to save anyway. We do not recommend saving with errors.