Running the Logic Checker - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

About this task

To run the Logic Checker:

Procedure

  1. Select the Logic Checker icon from the Toolbar.
  2. If the Logic Checker does not detect errors, a No Warnings Found dialog box appears. Click OK to return to the logic.
  3. If the Logic Checker detects errors, a Configuration Warnings Were Found dialog box appears. After you click OK, the tool returns you to the logic with Information symbols over the warning elements.
    Note: The Information symbols remain unless you ignore them and save the logic or fix the errors and run the Logic Checker successfully.