Editing TMR (Timer) Blocks - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

About this task

To edit TMR (Timer) blocks in Edit mode:

Procedure

  1. Double-click a Timer block. The TMR dialog box appears.
  2. Edit the timing functions of the block.
    Table 1. TMR (Timer) Block Configuration

    Field

    Description

    Duration

    Specifies the length of the timer function in seconds. The range is 5–86,400 seconds.

    Setup

    Determines the type of timer you use:

    • Pulse
    • On Delay
    • Off Delay
    • Minimum On
    • Minimum Off

    OK

    Accepts changes.

    Cancel

    Cancels changes.