Editing System Blocks - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

About this task

To edit System Blocks in Edit mode:

Procedure

  1. Double-click a System block. The Expose Attributes dialog box appears.
  2. Configure the inputs, outputs, and attributes of the subsystem.
    Note:
    • Select the Add button to add an attribute to configure. To remove attributes from the System, select the check box next to one or more attributes and click the Remove button.
    • To view the control system for the System block, drag and drop the control system from the Navigation Tree to the Panel Layout.
    • If you click Cancel to disregard your changes to the System block the changes are not saved, as expected. However, if you once again edit the same System block, and an error prompt appears stating An error occurred. Object does not exist, simply try these steps again. The error does not reoccur with the second attempt.