Editing Selector Blocks - Metasys - LIT-12011942 - Software Application - ODS Server - 10.1

Metasys Open Data Server Help

Brand
Metasys
Product name
ODS Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14
Language
English

About this task

To edit Selector blocks in Edit mode:

Procedure

  1. Double-click a Selector (Mux) block. The Selector Edit dialog box appears.
  2. Edit the fields and configure the number of inputs, the enumeration set, and the mode for each input.
    Table 1. Selector Block Configuration

    Field

    Description

    Input

    The number of inputs determines the list of inputs.

    Enum Category

    Filters the enumeration set list based on the chosen category.

    Enum Set

    When Enum Set changes, all modes are reset.

    Input 1 Mode(s)

    Click the button and a dialog box appears that allows you to select which modes associate with each input. In the dialog box, select the check box next to the desired mode(s). If a mode is already assigned to another input, the mode appears dimmed. Select Default to select all modes for an input that are not currently selected by any other input.

    Input 2 Mode(s)

    Click the button and a dialog box appears that allows you to select which modes associate with each input. In the dialog box, select the check box next to the desired mode(s). If a mode is already assigned to another input, the mode appears dimmed. Select Default to select all modes for an input that are not currently selected by any other input. There is one of these per input (2–8).

    OK

    Accepts changes.

    Cancel

    Cancels changes.