Editing Psychrometric Blocks - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

About this task

To edit Psychrometric blocks in Edit mode:

Procedure

  1. Double-click a Psychrometric block. The configuration dialog box appears.
  2. Edit the fields and configure the elevation based on the selected logic type.
    Note: If you double-click an ABH or DP block, the Unit Type field does not appear.
    Table 1. Psychrometric Block Configuration

    Field

    Description

    Elevation

    Allows you to configure the current elevation of the site (in feet or meters).

    Unit Type

    Allows you to choose International System of Units (SI) or Imperial (IP) units.

    Units for Unit Type SI are kilograms of water per kilogram of dry air.

    Units for Unit Type IP are pounds per cubic foot.

    OK

    Accepts changes.

    Cancel

    Cancels changes.