Editing Constant Enum - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14
Table 1. Constant Enum

Callout

Description

Enum Category

Set category determined by the user interface (either Two State or Multi State).

Enum Set

Set determined by the category selected in Enum Category.

Enum

Set state determined by the set and set category.

OK

Accepts changes.

Cancel

Cancels changes.