Editing Span Blocks - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

About this task

To edit Span blocks in Edit mode:

Procedure

  1. Double-click a Span block. The Span dialog box appears.
  2. Edit the fields to enable or disable clamping.
    Table 1. Span Block Configuration

    Field

    Description

    Clamp High

    Selects whether (True) or not (False) to clamp the Output at the Output High (OH). For more information on clamping, see Span.

    Clamp Low

    Selects whether (True) or not (False) to clamp the Output at the Output Low (OL). For more information on clamping, see Span.

    OK

    Accepts changes.

    Cancel

    Cancels changes.