Editing Bool Blocks - Metasys - LIT-12011942 - Software Application - ODS Server - 10.1

Metasys Open Data Server Help

Brand
Metasys
Product name
ODS Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14
Language
English

About this task

Note: LTCH (Latch) blocks are not editable.

To edit Bool blocks in Edit mode:

Procedure

  1. Double-click a Bool block. The configuration dialog box appears.
  2. Edit the fields and configure the number of inputs based on the selected type of Boolean logic.
    Table 1. Bool Block Configuration

    Field

    Description

    Input

    The number of inputs depends on the type of Bool block you use. You cannot reduce the input count lower than the number of current connections.

    OK

    Accepts changes.

    Cancel

    Cancels changes.