|
Field |
Description |
|---|---|
|
Label |
Enter a label here for the block.
Note: Do not start labels with a number and then follow it with any of these characters: $ . - ,
|
|
Object |
Browses to the object to which the reference is linked. Leaving this field blank leaves a placeholder for a future reference. The dragged object’s name appears in this field and the object’s attributes appear in the drop-down list in the attribute field. |
|
Attribute |
The attribute to which the reference is linked. When you are configuring an Output reference, the drop-down list contains numeric, writable attributes only. |
|
OK |
Accepts changes. |
|
Cancel |
Cancels changes. |