Editing Attribute Outputs - Metasys - LIT-12011942 - Software Application - ODS Server - 10.1

Metasys Open Data Server Help

Brand
Metasys
Product name
ODS Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14
Language
English
Table 1. Attribute Output

Field

Description

Name

Name of the output

Units

The units for the output

Display Precision

Tells the Metasys software what precision to use when formatting data.

This field only appears for floating outputs.
Note: Display Precision is used in the Focus view of data, not the graphical view.

Enum Category

Set category determined by the user interface (either Two State or Multi State).

This field only appears for Enum outputs.

Enum Set

Set determined by the category selected in Enum Category.

This field only appears for Enum outputs.

OK

Accepts changes.

Cancel

Cancels changes.