Editing Attribute Inputs - Metasys - LIT-12011942 - Software Application - ODS Server - 10.1

Metasys Open Data Server Help

Brand
Metasys
Product name
ODS Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14
Language
English
Table 1. Attribute Input

Field

Description

Name

Name of the input

Units

The units for the output.

This field only appears for floating inputs.

Display Precision

Tells the Metasys software what precision to use when formatting data.

This field only appears for floating inputs.
Note: Display Precision is used in the Focus view of data, not the graphical view.

Enum Category

Set category determined by the user interface (either Two State or Multi State).

This field only appears for Enum inputs.

Enum Set

Set determined by the category selected in Enum Category.

This field only appears for Enum inputs.

Trigger

This is checked if you want the attribute to trigger the control system to execute if its value changes by more than the defined increment.

OK

Accepts changes.

Cancel

Cancels changes.