Re-Routing a Connection - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

Procedure

  1. Make sure the LCT is running in Edit Mode.
  2. Place the cursor over an existing end connection point until the cursor changes into a cursor with lines protruding from the tip.
    Note: You may only move the destination point. To completely change the connection, see Deleting Connections.
  3. Click the connection point. The tool removes the connection.
  4. Click a new connection point. The tool creates the newly routed connection.