Drag and Drop - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

About this task

To add items to a control system using the drag and drop method:

Procedure

  1. In the Edit Mode of the LCT, left-click and drag an item from the left side of the tool view and drop it in the workspace.

    Notes:

    • If the item is a System block, a configuration wizard appears. Answer the questions to set up the new object/system or create a reference to an object or control system.
    • There is not interaction between the user navigation tree and logic.
  2. Edit the block to match your needs. See Editing Blocks in Edit Mode.