Copy and Paste - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

About this task

Note: You can copy and paste existing objects into the workspace from the workspace only.

To add items to a control system using the copy and paste method:

Procedure

  1. Right-click an existing object and select Copy.
  2. Right-click in the workspace and Paste the object.
    Note: The copy and paste method supports copying and pasting of multiple blocks. To copy and paste more than one block, hold down the Shift key while selecting blocks with the cursor or use the select tool to lasso the blocks.