Printing - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

The Logic Connector Tool supports printing of the following paper sizes in either landscape or portrait orientation:

  • Letter (8.5 x 11 in)

  • Folio (8.5 x 13 in)

  • Legal (8.5 x 14 in)

  • Tabloid (11 x 17 in)

  • A1

  • A2

  • A3

  • A4

  • A5

The Logic Connector Tool supports printing of just the existing control system.