This table describes the components of the TMR blocks:
|
Output |
Description |
|---|---|
|
IN |
Input |
|
RS |
Reset. Cancels the timer. Reset does not apply to Minimum On or Minimum Off timers. Use a binary object attribute for Reset (1.0=Reset Active, 0.0=Reset Inactive). |
The LCT contains five different types of timers. Each type uses a Duration (how long the timer is active) and unique functions to generate an Output. The different types of timers are listed below. Click the name of the timer for a description and figure of timer operation.
For information on setting Duration and the type of Timer, see Editing Timing Blocks.