Minimum On Timer Function - Metasys - LIT-12011942 - Software Application - ODS Server - 10.1

Metasys Open Data Server Help

Brand
Metasys
Product name
ODS Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14
Language
English

The following table and figures illustrate the function of the Minimum On timer.

Table 1. Minimum On Timer Function

Feature

Description

Activation

See row below.

Output

Goes active when there is a low to high Input transition when the timer executes (logic executes every 5 seconds). The Output remains active until the time specified in Duration passes AND the Input returns to inactive.

Reset

Has no effect on Minimum On timer.

Example

Keeps a chiller running for a minimum time after startup to stabilize equipment.

Figure 1. Minimum On Timer Example 1

Figure 2. Minimum On Timer Example 2