Statistical Category - Metasys - LIT-12011942 - Software Application - ODS Server - 10.1

Metasys Open Data Server Help

Brand
Metasys
Product name
ODS Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14
Language
English

Statistical blocks perform statistics on input. The number of inputs to a Statistical logic block depends on the number of inputs supported by the type of statistic. The Logic Connector Tool allows you to add multiple connections to the output of the block.

Table 1. Statistical Block Connections

Statistical Type

Inputs

AVG

2–8

MAX

2–8

MIN

2–8

See Editing Blocks in Edit Mode for information on editing Statistical blocks.