Math Category - Metasys - LIT-12011942 - Software Application - ODS Server - 10.1

Metasys Open Data Server Help

Brand
Metasys
Product name
ODS Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14
Language
English

Math blocks perform calculations on input. See the following table for details.

Table 1. Math Blocks

Block

Math Type

Inputs

*

Multiply

2–8

+

Add

2–8

X/Y

Divide

2

X-Y

Subtract

2

Neg

Negative

1

Abs

Absolute

1

Sqr

Square Root

1

Cos

Cosine

1

Sin

Sine

1

Tan

Tangent

1

ATan

Arc Tangent

1

ACos

Arc Cosine

1

ASin

Arc Sine

1

Exp

Exponent

1

LN

Natural Log

1

LOG

Log

1

X^Y

X^Y

2

The number of inputs to a Math logic block depends on the number of inputs supported by the type of math function. The Logic Connector Tool allows you to add multiple connections to the output of the block.

Note: Trigonometry blocks (SIN, COS, TAN, ASIN, ACOS, ATAN) perform calculations based on radians only.

See Editing Blocks in Edit Mode for information on editing Math blocks.