Constant Category - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

Constant logic blocks can have multiple connections to the output of the block. Constant logic blocks can be any one of the following:

Table 1. Constant Blocks

Block

Statistical Type

Enum

Enumeration

Float

Float

Rel.

Release

Note: Sends the Release command at a specific priority based on the connection.

See Editing Blocks in Edit Mode for information on editing Constant blocks.