Bool Category - Metasys - LIT-12011942 - Software Application - ODS Server - 10.1

Metasys Open Data Server Help

Brand
Metasys
Product name
ODS Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14
Language
English

Bool blocks apply Boolean functions to input. The number of inputs to a Bool logic block depends on the number of inputs supported by the type of Boolean function. The Logic Connector Tool allows you to add multiple connections to the output of the block.

Table 1. Bool Blocks

Bool Type

Inputs

AND

2–8

OR

2–8

XOR

2

NOT

1

LTCH

See LTCH (Latch) for details.

See Editing Blocks in Edit Mode for information on editing Bool blocks.