Logic Connector Tool Workspace - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

The Logic Connector Tool runs inside an active display panel. The workspace for the Program (Control System) Object defaults to a white background. You have the option to add a lined or dotted grid to the workspace using the appropriate buttons on the Toolbar. The workspace displays all building blocks and the connections between them, and serves as the destination for dragged and dropped blocks.