Logic Checker - Metasys - LIT-12011942 - Software Application - ODS Server - 10.1

Metasys Open Data Server Help

Brand
Metasys
Product name
ODS Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14
Language
English

The Logic Checker is not the same logic check run with a LCT save. It must be selected from the Toolbar. The Logic Checker scans the control system logic and reports any configuration issues it finds.

Table 1. Logic Checker

Condition

Message Text

Message Text Position

An output is not connected.

Missing Output Connection

Top-center of the block

An input is not connected.

Missing Input Connection

Top-center of the block

A feedback loop exists in the logic.

Feedback Loop Is Present

Top-center of a connection in the loop

An attribute is not connected.

Attribute Is Not Connected

Top-center of the attribute

Duplicate attribute name is defined.

Duplicate Attribute Name

Top-center of the attribute