Logic - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

Logic contains the following components:

Once a logic process completes, it runs again in approximately 5 seconds. For example, if a logic process starts at 10:00:00 and completes at 10:00:04, it runs again at 10:00:09. It is important that control applications that require particular timing use internal logic to determine time between execution.

If your logic references multiple Engines or multiple ODSs, and one device needs to be downloaded, upload all Engines and ODSs prior to making changes in SCT. This procedure ensures your logic works consistently.