LCT Modes - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

The Logic Connector Tool runs in either Edit Mode or View Mode.

You can generate logic and make logic changes when you are using Metasys in offline mode (using the SCT) or online mode. (See Metasys Modes.) After generating logic or making any changes to existing logic in offline mode, download the database to the online device to ensure the latest information is used.