Connections - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

Connection lines connect blocks in the logic. The LCT does not do a datatype check; that is, you can connect Boolean and Constant values, and any other combination. But, the tool does not allow inputs to connect to inputs, or outputs to outputs. The tool determines the connection line routing, and the only way to change the routing is to move the blocks or use the hide feature.