Average Output Computation - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

In the case of binary types of input references, if the majority of inputs are at State 1 or the inputs are evenly split between State 1 and State 0, the Average output is commanded to State 1. If the majority of inputs are at State 0, the Average output is commanded to State 0.