Signal Select Commands - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

The table below lists the commands supported by the Signal Select Object.

Table 1. Signal Select Object Commands

Command Name

Parameters

Description

Disable

None

Locks out all outputs and prevents the Signal Select functionality.

Enable

None

Ensures object reacts to any changes it may have missed while it was disabled and returns it to normal operation.