Signal Select Object - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document type
User Guide
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

Menu Selection: Insert > Object > Signal Select

The Signal Select object can process values from multiple zones to adjust various setpoints and can function with either analog or binary points.

For analog point types, the Signal Select object determines (one or more of) the low input, average input, and/or high input values for use in updating an attribute value of another object.

For binary point types, the Signal Select object determines (one or more of) the average state, the logical Or state, and/or the logical And state values for use in updating an attribute value of another object.

Computations take place at startup and at each time an input value experiences a change in value or reliability. The results of these calculations are sent to specified output points as commands. For example, this object allows you to average multiple zone temperatures and base a control, such as adjusting a setpoint, on that average.