Pulse Meter Commands - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

The table below lists the commands supported by the Pulse Meter Object.

Table 1. Pulse Meter Object Commands

Command Name

Parameters

Command Description

Enable

None

Enables the calculation of the pulse count and consumption for the Pulse Meter object.

Disable

None

Disables the calculation of the pulse count and consumption for the Pulse Meter object.

Reset

None

Resets the Pulse Meter, including the Consumption attribute.

Start Meter

None

Resumes metering.

Stop Meter

None

Stops metering.