Building an Optimal Start Application - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

About this task

To build an Optimal Start application:

Procedure

  1. Add the N2 Controller object and the analog and binary objects required for the OST application to the database. See the Object Help section for information on objects and the table in the Welcome section for information on the SCT. See Creating Items with Wizards for information on creating objects and other items.
  2. Add the Schedule Object (see Scheduling), referencing the binary object controlling Zone Occupancy Mode.
  3. Make sure valid occupied and unoccupied times are entered into the Schedule object.
  4. Add the Optimal Start Object referencing the above Schedule object, the Binary objects designated as Zone Occupancy Mode and Zone Warmup or Cooldown Mode, and the analog attributes of objects designated as temperatures and setpoints.

Results

Note: See the User Interface section for information on creating, editing, commanding, and deleting objects. See the Scheduling section for information on scheduling.