Optimal Start Commands - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

The table below lists the commands supported by the Optimal Start Object.

Table 1. Optimal Start Object Commands

Command Name

Parameters

Command Description

Cancel Prestart

None

Delays pending start until latest prestart time. Only valid during Prestart and before the optimal start time.

Cancel Prestop

None

Cancels the pending stop. Only valid during Prestop and before the optimal stop time.

Disable

None

Prevents the object’s functionality; no calculations take place.

Enable

None

Allows the object to perform its calculations once a minute.