Remote Services Connection Tab - Metasys - LIT-12011942 - Software Application - Metasys Open Data Server - 10.1

Metasys Open Data Server Help

Product
Building Automation Systems > Databases and Data Servers > Metasys Open Data Server
Document number
LIT-12011942
Version
10.1
Revision date
2019-10-14

The Remote Services Connection tab resides on the Site Object and enables you to connect to the cloud-based platform. Starting at Release 10.0, you can no longer configure a connection to a cloud-based platform with the attributes in the Remote Services Connection tab of the Site object. The tab is appears but its attributes should no longer be defined.